FB#.RESKTR
Description
This parameter sets the resolver nominal transformation ratio. It affects the resolver excitation output amplitude.
The value is obtained from the resolver data sheet.
Context
See Feedback # View.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0.001 to 50.000 |
|
Default Value |
0.5 |
|
Data Type |
Float |
|
See Also |
N/A |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
FB1.RESKTR |
3500h |
04h |
Unsigned16 |
- |
1000:1 |
Read/Write |
No |
|
FB2.RESKTR |
3501h |
04h |
Unsigned16 |
- |
1000:1 |
Read/Write |
No |
|
FB3.RESKTR |
3502h |
04h |
Unsigned16 |
- |
1000:1 |
Read/Write |
No |
|
FB4.RESKTR |
3503h |
04h |
Unsigned16 |
- |
1000:1 |
Read/Write |
No |
|
FB5.RESKTR |
3504h |
04h |
Unsigned16 |
- |
1000:1 |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
30140 |
1 |
30140 (0x75bc) |
FB1.RESKTR |
Unsigned16 |
Read/Write |
Yes |
|
30141 |
1 |
30141 (0x75bd) |
FB2.RESKTR |
Unsigned16 |
Read/Write |
Yes |
|
30142 |
1 |
30142 (0x75be) |
FB3.RESKTR |
Unsigned16 |
Read/Write |
Yes |
|
30143 |
1 |
30143 (0x75bf) |
FB4.RESKTR |
Unsigned16 |
Read/Write |
Yes |
|
30144 |
1 |
30144 (0x75c0) |
FB5.RESKTR |
Unsigned16 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
FB1.RESKTR |
30140 |
Float |
Read/Write |
- |
|
FB2.RESKTR |
30141 |
Float |
Read/Write |
- |
|
FB3.RESKTR |
30142 |
Float |
Read/Write |
- |
|
FB4.RESKTR |
30143 |
Float |
Read/Write |
- |
|
FB5.RESKTR |
30144 |
Float |
Read/Write |
- |